Back

Haas Basic Mill Operator

Below is the Basic Mill Operator Course Curriculum. Please review the following points, prior to starting this course:

Courses are presented one chapter at a time, with individual topics presented in video format. Each video is followed by a corresponding quiz to test your understanding of the topic presented. You must pass the quiz for each topic to gain access to the next topic.

  • Start by viewing the Introduction to Haas Certification video below (there is no corresponding quiz)
  • To begin your course, select the first topic in Chapter 1, watch the video, and take the quiz
  • Once you have clicked the Take Quiz button, you will have 15 minutes to complete the quiz
  • You must score 100% on each quiz to pass, and gain access to the next topic; if you fail a quiz, you must retake it until you pass
  • Quizzes are straightforward, and based solely on the content presented in the corresponding video – there are no trick questions
  • Best of luck on your journey through the Haas Certification Program!

Diego Ruvalcaba - Haas Basic Mill Operator Feedback

Diego was able to select the correct martial from the drawing.

He cleaned the vise and loaded the stock in the vise against the stop with the correct pressure.

Using single block, distance to go and setting the rapid overrides safely start the program.

Diego pulled up on the vise handle when tightening the vise.  I recommended that he switch the handle so he can push down with both hands on the handle to loosen and tighten the vise.

 

Josh Huffaker - Haas Basic Mill Operator Feedback

Joshua,

          Selected the correct material for the part and was able to load the vise correctly.

He started the program safely using single block watching the distance to go position at 5% rapid.

He also knew the control key functions and knew that he should not touch the overrides buttons.

You can tell he had no experience running the actual machine and can use some practice to get more comfortable load the part.

-Ernie

Javier Santillana - Haas Basic Mill Operator Feedback

Javier,

          Selected the correct material for the part and was able to load the vise correctly.

He started the program safely using single block watching the distance to go position at 5% rapid.

He also knew the control key functions and knew that he should not touch the overrides buttons.

You can tell he had little experience running the actual machine and can use some practice to get more comfortable load the part.

-Ernie