Back

Javier Santillana - Haas Basic Mill Operator Feedback

Javier,

          Selected the correct material for the part and was able to load the vise correctly.

He started the program safely using single block watching the distance to go position at 5% rapid.

He also knew the control key functions and knew that he should not touch the overrides buttons.

You can tell he had little experience running the actual machine and can use some practice to get more comfortable load the part.

-Ernie

 

Result: 
Passed
Trainee User: 
Certificate Hash: 
b5f0fb9ab
Certification Center: 
Test Machining School of California