Back

Josh Huffaker - Haas Basic Mill Operator Feedback

Joshua,

          Selected the correct material for the part and was able to load the vise correctly.

He started the program safely using single block watching the distance to go position at 5% rapid.

He also knew the control key functions and knew that he should not touch the overrides buttons.

You can tell he had no experience running the actual machine and can use some practice to get more comfortable load the part.

-Ernie

Result: 
Passed
Trainee User: 
Certificate Hash: 
2bc1d25be
Certification Center: 
Test Machining School of California